1.2.27.1 WDT_Initialize Function
C
void WDT_Initialize( void )
Summary
Initializes given instance of the WDT peripheral.
Description
This function initializes the given instance of the WDT peripheral as configured by the user.
Precondition
None.
Parameters
None.
Returns
None.
Example
WDT_Initialize();
Remarks
The WDT peripheral is also configured by setting in the NVM User Row. These settings are specified though compiler provided fuse settings.