1.38.10.2 FREQM_MeasurementStart Function
C
bool FREQM_MeasurementStart(void)
Summary
This function starts the frequency measurement.
Description
This function starts the frequency measurement. This function is always non-blocking. Calling this function when a frequency measurement is already in progress will result in a functional no operation. The FREQM_IsBusy() function will return true when a frequency measurement is in progress. The completion of the measurement operation is indicated by the FREQM_IsBusy() function returing false or a registered callback function being called.
Precondition
FREQM module should be initialized with the required configuration parameters from the MHC GUI in the FREQM_Initialize() function
Parameters
None
Returns
Returns false if the peripheral is busy
Example
bool status = false; status = FREQM_MeasurementStart();
Remarks
None.