1.20.10.3 ICAPx_Error_CallbackRegister Function
C
/* x = ICAP instance number */
void ICAPx_Error_CallbackRegister(ICAP_CALLBACK callback, uintptr_t context)
Summary
Sets the callback function for a ICAP error interrupt.
Description
This function sets the callback function that will be called when the ICAP error occurs.
Precondition
ICAPx_Initialize() function must have been called first.
Parameters
Param | Description |
---|---|
callback | a pointer to the function to be called when value is reached. Use NULL to Unregister the compare callback |
context | a pointer to user defined data to be used when the callback function is called. NULL can be passed if no data needed |
Returns
None.
Example
void APP_ICAPTransferHandler(uintptr_t context)
{
}
ICAP1_Error_CallbackRegister(&APP_ICAPTransferHandler, (uintptr_t)NULL);
Remarks
None