1.7.1.4 AC_SetVddScalar Function
C
void AC_SetVddScalar (AC_CHANNEL channel_id , uint8_t vdd_scalar)
Summary
Sets VDDSCALER value of a comparator.
Description
This function sets VDDSCALERn of a comparator. The VDDSCALERn associated with a comparator (COMPn) can be used as one of the inputs to the comparator. This allows to set flexible compare voltages.
Precondition
AC_Initialize must have been called for the associated AC instance.
Parameters
Param | Description |
---|---|
channel | Points to AC Channel |
vdd_scalar | Scaling factor (6-bits) ranges from 0 to 63. |
Returns
None.
Example
AC_SetVddScalar (AC_CHANNEL_0, 0x0B);
Remarks
None.