1.3.14.4 NVIC_INT_Restore Function

C

bool NVIC_INT_Restore( bool state );

Summary

Enables or Disables all global interrupts based on PRIMASK bit state

Description

This function enables or disables all global interrupts based on the Priority Mask Register (PRIMASK) bit status.

The bit status returned from NVIC_INT_Disable() API should be passed to this function.

  • If the state is true then it enables all the global interrupts

  • If the state is false then it disables all the global interrupts

Precondition

None.

Parameters

Param Description
state Specifies whether to enable or disable global interrupts.

Returns

None.

Example

bool intState = NVIC_INT_Disable();

NVIC_INT_Restore(intState);

Remarks

None.