1.14.3.2 CDACx_DataWrite Function

C

// x is instance of the peripheral and it is applicable only for devices having multiple instances of the peripheral.
void CDACx_DataWrite( uint16_t data )

Summary

This function will write the specified value to the CDAC and start the conversion.

Description

This function will write the specified value to the CDAC and start the conversion. The internal and/or external CDAC outputs will be updated if these output were enabled. The analog output voltage will depend on the choice of the CDAC reference.

Precondition

CDACx_Initialize must have been called for the associated CDAC instance.

Parameters

Param Description
data Digital value to be converted.

Returns

None.

Example

uint16_t data = 0x800;
CDAC1_Initialize();
CDAC1_DataWrite(data);

Remarks

None.