1.36.15.10 RTT_TimerValueGet Function
C
uint32_t RTT_TimerValueGet(void);
Summary
Returns the current timer value
Description
This function is used the counter value of RTT. This value can be use to calculate the time elapsed.
Precondition
None.
Parameters
None.
Returns
The current timer count
Example
uint32_t frequency = 0; uint32_t count = 0; uint64_t time_elapsed; frequency = RTT_FrequencyGet(); count = RTT_TimerValueGet(); time_elapsed = count/frequency;