1.18.5.7 CORETIMER_FrequencyGet Function
C
uint32_t CORETIMER_FrequencyGet(void);
Summary
Provides the given Core timer's counter-increment frequency.
Description
This function provides the frequency at which the given counter increments. It can be used to convert differences between counter values to real time or real-time intervals to timer period values.
Precondition
CORETIMER_Initialize() function must have been called first.
Parameters
None.
Returns
frequency - The frequency (in Hz) at which the timer counter increments.
Example
uint32_t frequency; CORETIMER_Initialize(); frequency = CORETIMER_FrequencyGet();
Remarks
Should be generated for interrupt mode only.