1.16.21.23 UARTx_ReadAbort Function
C
/* x = UART instance number */
/* Non-blocking mode */
bool UARTx_ReadAbort(void)
Summary
Aborts the ongoing read request
Description
This API lets the application abort an ongoing read request. If needed, the application can call the UARTx_ReadCountGet API to know the number of bytes successfully read before issuing the UARTx_ReadAbort API.
Precondition
UARTx_Initialize must have been called for the associated UART instance.
Parameters
None
Returns
true - operation is successful
false - error during execution
Example
bool timeout; if (timeout == true) { // Kill the ongoing read read request UART1_ReadAbort(); }
Remarks
None