1.42.19.5 SYSTICK_TimerPeriodSet Function
C
void SYSTICK_TimerPeriodSet( uint32_t period )
Summary
Set the SysTick Load Value
Description
This function is used to update SysTick Load value
Preconditions
Systick should be stopped prior to setting up the new Load value by calling SYSTICK_TimerStop. This will make sure that the new value is used for the next Tick
Parameters
Param | Description |
---|---|
period | The period is specified as a number of clock ticks between SysTick interrupt. It must be between 1 and 16,777,216, inclusive. |
Returns
None.
Example
SYSTICK_TimerStop();
SYSTICK_TimerPeriodSet(0x00004567);
SYSTICK_TimerStart();