1.37.1.2 AC_CallbackRegister Function
C
void AC_CallbackRegister (AC_CALLBACK callback, uintptr_t context)
Summary
Allows application to register callback with PLIB
Description
This function allows application to register a callback function for the PLIB to call back when interrupt occurred.
At any point if application wants to stop the callback, it can call this function with "callback" value as NULL.
Precondition
AC_Initialize must have been called for the associated AC instance.
Parameters
Param | Description |
---|---|
callback | Pointer to the callback function implemented by the user. |
context | The value of parameter will be passed back to the application unchanged, when the callback function is called. It can be used to identify any application specific value that identifies the instance of the client module (for example, it may be a pointer to the client module's state structure) |
Returns
None.
Example
uintptr_t comparator_context;
void ac_callBack(uint8_t int_flag, uintptr_t ac_context)
{
// Check the comparator output state
if(int_flag & AC_STATUSA_STATE0_Msk)
{
...
}
}
// Add the following after SYS_Initialize (NULL) in the main code
AC_CallbackRegister(ac_callBack, comparator_context);
Remarks
None.