1.18.12.2 OCMPx_FaultStatusGet Function
C
/* x = OCMP instance number */ bool OCMPx_FaultStatusGet (void)
Summary
Reads the fault status
Description
Returns the current state of the fault condition. When fault is detected, the PWM outputs are shut down asynchronously.
Precondition
OCMPx_Initialize() function must have been called first.
Parameters
None.
Returns
bool - status of the fault pin.
Example
bool status; OCMP1_Initialize(); OCMP1_Enable(); status = OCMP1_FaultStatusGet();
Remarks
This function is applicable only for output compare mode (OCM) = 7 which is PWM mode with fault enabled