1.20.8.12 GPIO_PinWrite Function
C
void GPIO_PinWrite(GPIO_PIN pin, bool value)
Summary
Writes the logic level of the selected pin.
Description
This function writes/drives the "value" on the selected I/O line/pin.
Precondition
The desired pin must be configured as an output pin.
Parameters
Param | Description |
---|---|
pin | One of the IO pins from the enum GPIO_PIN |
value | value to be written on the selected pin: |
- true | set pin to high (1). |
- false | clear pin to low (0). |
Returns
None.
Example
GPIO_PinWrite(GPIO_PIN_RB3, true);
Remarks
None.