1.24.9.23 GPIO_PinIntDisable Function

C

void GPIO_PinIntDisable(GPIO_PIN pin);

Summary

Disables IO interrupt on selected IO pin.

Description

This function disables IO interrupt on selected IO pin.

Precondition

  • Corresponding pin must be configured in interrupt mode in MHC Pin Manager.

  • GPIO_Initialize() must have been called.

Parameters

Param Description
pin One of the IO pins from the enum GPIO_PIN

Returns

None.

Example

GPIO_PinIntDisable(GPIO_PIN_RB3);

Remarks

None.