3.41.19 Supply Controller (SUPC)
The Supply Controller (SUPC) controls the supply voltages of the system. The SUPC also generates the slow
clock by selecting either the low-power RC oscillator or the low-power crystal oscillator.
Using The Library
Configure the peripheral library using the MCC.
Library Interface
Supply Controller peripheral library provides the following interfaces:
Functions
Name | Description |
---|---|
SUPC_Initialize | Initializes SUPC module of the device |