21.4.3 Processor-Specific Macros

The proc/p*.h header files define a number of processor-specific macros. To use these macros, #include <xc.h> in your source file. This list is not comprehensive.

__PIC32_HAS_L1CACHEDefined if and only if the target device supports an L1 cache
__PIC32_HAS_MIPS32R2Defined if and only if the target device supports the MIPS32r2 Instruction Set
__PIC32_HAS_MICROMIPSDefined if and only if the target device supports the microMIPS32 Instruction Set
__PIC32_HAS_MIPS16Defined if and only if the target device supports the MIPS16 Instruction Set
__PIC32_HAS_DSPR2Defined if and only if the target device supports the DSP-enhanced core
__PIC32_HAS_FPU64Defined if and only if the target device supports the 64-bit Hardware Floating-Point Unit. Also check __mips_hard_float to determine if the compiler is set to compile for the FPU.
_<Interrupt-Source>_VECTORDefined to the vector number for the interrupt source and intended to be used with the vector function attribute. for example, #define _CORE_TIMER_VECTOR 0
_<Interrupt-Source>_IRQDefined to the IRQ number for the interrupt source. for example, #define _CORE_SOFTWARE_0_IRQ 1
_<SFR>_<Bitfield>_POSITIONDefined to the position of a bitfield within a special function register (SFR). for example, #define _WDTCON_ON_POSITION 0x0000000F
_<SFR>_<Bitfield>_MASKDefined to a mask of the bitfield within a special function register (SFR). for example, #define _WDTCON_ON_MASK 0x00008000
_<SFR>_<Bitfield>_LENGTHDefined to the length of the bitfield within a special function register (SFR). for example, #define _WDTCON_ON_LENGTH 0x00000001
<Special-Function-Register>Defined to the Special Function Register name. for example, #define T5CON T5CON

This macro allows preprocessor testing for the existence of an SFR before using it. For example:

#if defined(T5CON)
  T5CONbits.ON = 1;
#endif