21.4.2 SDE Compatibility Macros
The MIPS® SDE (Software Development Environment) defines a number of
macros, most with the prefix “_MIPS_”, which characterize various target specific
options, some determined by command line options (for example,
-mint64). Where applicable, these macros will be defined by the
compiler in order to ease porting applications and middleware from the SDE to the
compiler.
_MIPS_SZINT | |
_MIPS_SZLONG | |
_MIPS_SZPTR | |
__mips_no_float | |
__mips__
| Always defined. |
R3000
| Defined if -ansi is not specified. |
_mips_fpr | Defined as 32. |
__mips16 | Defined if -mips16 specified. |
__mips | Defined as 32. |
__mips_isa_rev | Defined as 2. |
_MIPS_ISA | Defined as _MIPS_ISA_MIPS32. |