22.3.3 Processor Definitions Include File for PIC32MX Family
The next line in the default linker script pulls in information specific to the processor.
INCLUDE procdefs.ld
The file procdefs.ld is included in the linker script at
this point. The file is searched for in the current directory and in any directory
specified with the -L command line option. The compiler shell ensures
that the correct directory is passed to the linker with the -L command
line option based on the processor selected with the -mprocessor
command line option.
The processor definitions linker script contains the following pieces of information: