22.3.3.2 Optional Inclusion of Processor-Specific Peripheral Libraries

Note: The legacy peripheral libraries are deprecated and are replaced by the MPLAB Harmony libraries, installed separately.

This section of the processor definitions linker script ensures that the processor-specific peripheral libraries get included, but only if the files exist.

/*********************************************************************

 * Processor-specific peripheral libraries are
        optional

*********************************************************************/

OPTIONAL("libmchp_peripheral.a")

OPTIONAL("libmchp_peripheral_32MX795F512L.a")

The OPTIONAL lines specify that libmchp_peripheral.a and libmchp_peripheral_32MX795F512L.a should be included in the link as if the files were named on the command line. The linker attempts to find these files in the current directory. If they are not found in the current directory, the linker searches through the library search paths. If they are not found in the library search paths, the link process continues without error. The linker will error only when a symbol from the -peripheral library is required but not found elsewhere.