15.7 Function Return Values

Function return values are returned in registers.

Integral or pointer value are placed in register v0. All floating-point values, regardless of precision, are returned in floating-point register $f0.

If a function needs to return an actual structure or union – not a pointer to such an object – the called function copies this object to an area of memory that is reserved by the caller. The caller passes the address of this memory area in register $4 when the function is called. The function also returns a pointer to the returned object in register v0. Having the caller supply the return object’s space allows re-entrance.