15.1 Writing Functions
Functions may be written in the usual way in accordance with the C/C++ language.
The only specifier that has any effect on function is
static. Interrupt functions are defined with the use of the
interrupt attribute, see Function Attributes and Specifiers.
A function defined using the static specifier only affects
the scope of the function, that is, limits the places in the source code where the
function may be called. Functions that are static may only be directly
called from code in the file in which the function is defined. The equivalent symbol
used in assembly code to represent the function may change if the function is
static, see Static Variables. This specifier does not change the way the function is encoded.