9.8 Memory Models

MPLAB XC32 C/C++ Compiler does not use fixed memory models to alter allocation of variables to memory.

The -G option (see Options Specific to PIC32M Devices), which controls the gp-relative addressing threshold, is similar to the small-data/large-data/scalar-data memory models offered by the Microchip compilers for the 8- and 16-bit architectures. The value specified with this option indicates the maximum size of objects that will be allocated to the small data sections, for example, sbss, sdata, etc. Variables allocated to the small-data sections require fewer instructions to access than variables allocated to the other data sections. For example:
xc32-gcc -G128 -mprocessor=32MZ2048ECH100
                                        -mdfp="Microchip/Microchip.PIC32MZ-EC_DFP.1.4.150" main.c

In this example, data objects up to 128 bytes in size will be located in the efficient small-data or small-bss section.

In general larger -G values result in more efficient code. However, gp-relative addressing is limited to 64-KB of small data.