9.2 Variables in Data Memory

Most variables are ultimately positioned into the data memory. The exceptions are non-auto variables which are qualified as const, which are placed in the program memory space, see Const Type Qualifier.

Due to the fundamentally different way in which auto variables and non-auto variables are allocated memory, they are discussed separately. To use the C/C++ language terminology, these two groups of variables are those with automatic storage duration and those with permanent storage duration, respectively.

Note: The terms “local” and “global” are commonly used to describe variables, but are not ones defined by the language standard. The term “local variable” is often taken to mean a variable which has scope inside a function, and “global variable” is one which has scope throughout the entire program. However, the C/C++ language has three common scopes: block, file (that is, internal linkage) and program (that is, external linkage), so using only two terms to describe these can be confusing. For example, a static variable defined outside a function has scope only in that file, so it is not globally accessible, but it can be accessed by more than one function inside that file, so it is not local to any one function either. In terms of memory allocation, variables are allocated space based on whether it is an auto or not, hence the grouping in the following sections.