8.9.1 Const Type Qualifier

The const type qualifier is used to tell the compiler that an object is read only and must not be modified. The compiler will issue a warning or error if you attempt to modify an object declared const in source code.

A const object is usually defined with initial values, as the program cannot write to these objects at runtime. However this is not a requirement. An uninitialized const object is allocated space in one of the bss sections, along with other uninitialized RAM variables, but is still treated as read-only by the compiler.
const char IOtype = ’A’;  // initialized const object
const char buffer[10];    // I just reserve memory in RAM
Objects qualified only with const are not guaranteed to be located in program memory. The use of some options can affect where const-qualified object are located. Objects qualified const might be placed in data memory when the -fzero-initialized-in-bss, -fdata-sections, or -mno-embedded-data options are used. To explicitly request that the object be placed in program memory regardless of the usage of the options listed, use the space(prog) attribute along with the const qualifier (see Variables in Program Memory).