3.5.1 How Can I Make My Code Smaller?
There are a number of ways that this can be done, but results vary from one project to the next. Use the assembly list file to observe the assembly code produced by the compiler to verify that the following tips are relevant to your code. For information on the list file, see the MPLAB® XC32 Assembler, Linker and Utilities User’s Guide (DS50002186).
Use the smallest data types possible as less code is needed to access these (this also reduces RAM usage). For examples, a short integer type exists for this compiler. See Supported Data Types and Variables for all data types and sizes.
There are two sizes of floating-point type, which are discussed in the same section. Replace floating-point variables with integer variables wherever possible. For many applications, scaling a variable's value makes eliminating floating-point operations possible.
Use unsigned types, if possible, instead of signed types, particularly if they are used in expressions with a mix of types and sizes. Try to avoid an operator acting on operands with mixed sizes whenever possible.
for(i=0; i!=10; i++)is
preferable
to:for(i=0; i<10; i++)A check for equality (== or !=) is usually more efficient to implement than the weaker < comparison.
for(i=10; i!=0; i--)Choose the highest optimization level, -Os. (See Options for Controlling Optimization).
Consider also the standard link-time optimizer, controlled by the -flto option.
This optimization adds internal bytecode representations of the
code to special sections in the object file that are then
processed as if they had been part of the same translation unit.
This can allow the compiler to make certain assumptions about
the program code and improved the effectively of some
optimizations.
Consider using the a compressed ISA mode such as MIPS16 or microMIPS if it is supported on your device. Use the -mips16 or -mmicromips option for your project to make the compiler default to these modes. Use the mips16 or micromips function attributes to change the mode at the function level. You may also choose the optimized and compressed variants of the libraries in the linker options. Be aware of what optimizations the compiler performs so you can take advantage of them and don’t waste your time manually performing optimizations in C code that the compiler already handles, for example, don’t turn a multiply-by-4 operation into a shift-by-2 operation as this sort of optimization is already detected.