17.2.11 Initialize Bus Matrix Registers

On some of the PIC32 MCUs, the bus matrix registers (BMXDKPBA, BMXDUDBA, BMXDUPBA) must be initialized by the start-up code if any RAM functions exist. The startup code leaves these registers in their state when RAM functions do not exist in the projects. The linker collects all RAM functions and allocates them to a section of data memory that is aligned on a 2K-alignment boundary. To determine whether any RAM functions exist in the application, the linker provides a variable that contains the beginning address of this section. This variable is named _ramfunc_begin.

In addition, the linker provides a 2K-aligned variable required for the boundary register (BMXDKPBA). The variable is named _bmxdkpba_address. The linker also provides two variables that contains the addresses for the bus matrix register. These variables are named _bmxdkpba_address, _bmxdudba_address, and _bmxdupba_address.

The linker ensures that RAM functions are aligned to a 2K-alignment boundary as is required by the BMXDKPBA register.

On other PIC32 devices, no special bus initialization is required to execute RAM functions.

Figure 17-3. Bus Matrix Initialization

Initialize CP0 Registers

The CP0 registers are initialized in the following order:

  1. Count register
  2. Compare register
  3. EBase register
  4. IntCtl register
  5. Cause register
  6. Status register

Hardware Enable Register (HWREna – CP0 Register 7, Select 0)

This register contains a bit mask that determines which hardware registers are accessible via the RDHWR instruction. Privileged software may determine which of the hardware registers are accessible by the RDHWR instruction. In doing so, a register may be virtualized at the cost of handling a Reserved Instruction Exception, interpreting the instruction, and returning the virtualized value. For example, if it is not desirable to provide direct access to the Count register, access to the register may be individually dis-abled, and the return value can be virtualized by the operating system.

No initialization is performed on this register in the PIC32 start-up code.

Bad Virtual Address Register (BadVAddr – CP0 Register 8, Select 0)

This register is a read-only register that captures the most recent virtual address that caused an Address Error exception (AdEL or AdES).No initialization is performed on this register in the PIC32 start-up code.

Count Register (Count – CP0 Register 9, Select 0)

This register acts as a timer, incrementing at a constant rate, whether or not an instruction is executed, retired, or any forward progress is made through the pipeline. The counter increments every other clock if the DC bit in the Cause register is '0'. The Count register can be written for functional or diagnostic purposes, including at Reset or to synchronize processors. By writing the CountDM bit in the Debug register, it is possible to control whether the Count register continues incrementing while the processor is in Debug mode. This register is cleared in the default PIC32 start-up code.

Status Register (Status – CP0 Register 12, Select 0)

This register is a read/write register that contains the operating mode, Interrupt Enabling, and the diagnostic states of the processor. Fields of this register combine to create operating modes for the processor.

The following settings are initialized by the default PIC32 start-up code (0b000000000x0xx0?00000000000000000):

  • Access to Coprocessor 0 not allowed in User mode (CU0 = 0)
  • User mode uses configured endianess (RE = 0)
  • No change to exception vectors location (BEV = no change)
  • No change to flag bits that indicate reason for entry to the Reset exception vector (SR, NMI = no change)
  • Interrupt masks are cleared to disable any pending interrupt requests (IM7..IM2 = 0, IM1..IM0 = 0)
  • Interrupt priority level is 0 (IPL = 0)
  • Base mode is Kernel mode (UM = 0)
  • Error level is normal (ERL = 0)
  • Exception level is normal (EXL = 0)
  • Interrupts are disabled (IE = 0)

The DSPr2 engine is enabled on target devices featuring the DSPr2 engine (MX = 1).

The IEEE 754 compliant Floating-Point Unit is enabled for target devices that support the FPU. The FPU is configured in the FR64 mode, which defines 32 64-bit float-ing-point general registers (FPRs) with all formats supported in each register (CU1=1) and (FR=1).

Interrupt Control Register (IntCtl – CP0 Register 12, Select 1)

This register controls the expanded interrupt capability added in Release 2 of the Architecture, including vectored interrupts and support for an external interrupt controller.

This register contains the vector spacing for interrupt handling. The vector spacing portion of this register (bits 9..5) is initialized with the value of the _vector_spacing symbol by the PIC32 start-up code. All other bits are set to '1'.

Shadow Register Control Register (SRSCtl – CP0 Register 12, Select 2)

This register controls the operation of the GPR shadow sets in the processor. The default startup code uses the SRSCtl register when it initializes the Global Pointer register in all register sets. However, it restores the original SRSCtl value after the GP register is initialized.

Shadow Register Map Register (SRSMap – CP0 Register 12, Select 3)

This register contains eight 4-bit fields that provide the mapping from a vector number to the shadow set number to use when servicing such an interrupt. The values from this register are not used for a non-interrupt exception, or a non-vectored interrupt (CauseIV = 0 or IntCtlVS = 0). In such cases, the shadow set number comes from SRSCtlESS. If SRSCtlHSS is zero, the results of a software read or write of this register are UNPREDICTABLE. The operation of the processor is UNDEFINED if a value is written to any field in this register that is greater than the value of SRSCtlHSS. The SRSMap register contains the shadow register set numbers for vector numbers 7..0. The same shadow set number can be established for multiple interrupt vectors, creating a many-to-one mapping from a vector to a single shadow register set number.

No initialization is performed on this register in the PIC32 start-up code.

Cause Register (Cause – CP0 Register 13, Select 0)

This register primarily describes the cause of the most recent exception. In addition, fields also control software interrupt requests and the vector through which interrupts are dispatched. With the exception of the DC, IV, and IP1..IP0 fields, all fields in the Cause register are read-only. Release 2 of the Architecture added optional support for an External Interrupt Controller (EIC) interrupt mode, in which IP7..IP2 are interpreted as the Requested Interrupt Priority Level (RIPL).

The following settings are initialized by the PIC32 start-up code:

  • Enable counting of Count register (DC = no change)
  • Use the special exception vector (16#200) (IV = 1)
  • Disable software interrupt requests (IP1..IP0 = 0)

Exception Program Counter (EPC – CP0 Register 14, Select 0)

This register is a read/write register that contains the address at which processing resumes after an exception has been serviced. All bits of the EPC register are significant and must be writable. For synchronous (precise) exceptions, the EPC contains one of the following:

  • The virtual address of the instruction that was the direct cause of the exception
  • The virtual address of the immediately preceding branch or jump instruction, when the exception causing instruction is a branch delay slot and the Branch Delay bit in the Cause register is set.

On new exceptions, the processor does not write to the EPC register when the EXL bit in the Status register is set; however, the register can still be written via the MTC0 instruction.

No initialization is performed on this register in the PIC32 start-up code.

Processor Identification Register (PRId – CP0 Register 15, Select 0)

This register is a 32-bit read-only register that contains information identifying the manufacturer, manufacturer options, processor identification, and revision level of the processor.

No initialization is performed on this register in the PIC32 start-up code.

Exception Base Register (EBase – CP0 Register 15, Select 1)

This register is a read/write register containing the base address of the exception vectors used when StatusBEV equals 0, and a read-only CPU number value that may be used by software to distinguish different processors in a multi-processor system. The EBase register provides the ability for software to identify the specific processor within a multi-processor system, and allows the exception vectors for each processor to be different, especially in systems composed of heterogeneous processors. Bits 31..12 of the EBase register are concatenated with zeros to form the base of the exception vectors when StatusBEV is 0. The exception vector base address comes from fixed defaults when StatusBEV is 1, or for any EJTAG Debug exception. The Reset state of bits 31..12 of the EBase register initialize the exception base register to 16#8000-0000, providing backward compatibility with Release 1 implementations. Bits 31..30 of the EBase register are fixed with the value 2#10 to force the exception base address to be in KSEG0 or KSEG1 unmapped virtual address segments.

If the value of the exception base register is to be changed, this must be done with StatusBEV equal 1. The operation of the processor is UNDEFINED if the Exception Base field is written with a different value when StatusBEV is 0.

Combining bits 31..30 with the Exception Base field allows the base address of the exception vectors to be placed at any 4K byte page boundary. If vectored interrupts are used, a vector offset greater than 4K byte can be generated. In this case, bit 12 of the Exception Base field must be zero. The operation of the processor is UNDEFINED if software writes bit 12 of the Exception Base field with a 1 and enables the use of a vectored interrupt whose offset is greater than 4K bytes from the exception base address.

This register is initialized with the value of the _ebase_address symbol by the PIC32 start-up code. _ebase_address is provided by the linker script with a default value of the start of KSEG1 program memory. The user can change this value by providing the command line option -–defsym _ebase_address=A to the linker.

Config Register (Config – CP0 Register 16, Select 0)

This register specifies various configuration and capabilities information. Most of the fields in the Config register are initialized by hardware during the Reset exception pr-ocess, or are constant.

No initialization is performed on this register in the PIC32 start-up code.

Config1 Register (Config1 – CP0 Register 16, Select 1)

This register is an adjunct to the Config register and encodes additional information about the capabilities present on the core. All fields in the Config1 register are read-only.

No initialization is performed on this register in the PIC32 start-up code.

Config2 Register (Config2 – CP0 Register 16, Select 2)

This register is an adjunct to the Config register and is reserved to encode additional capabilities information. Config2 is allocated for showing the configuration of level 2/3 caches. These fields are reset to 0 because L2/L3 caches are not supported on the core. All fields in the Config2 register are read-only.

No initialization is performed on this register in the PIC32 start-up code.

Config3 Register (Config3 – CP0 Register 16, Select 3)

This register encodes additional capabilities. All fields in the Config3 register are read-only.

No initialization is performed on this register in the PIC32 start-up code.

Debug Register (Debug – CP0 Register 23, Select 0)

This register is used to control the debug exception and provide information about the cause of the debug exception, and when re-entering at the debug exception vector due to a normal exception in Debug mode. The read-only information bits are updated every time the debug exception is taken, or when a normal exception is taken when already in Debug mode. Only the DM bit and the EJTAGver field are valid when read from non-Debug mode. The values of all other bits and fields are UNPREDICTABLE. Operation of the processor is UNDEFINED if the Debug register is written from non-Debug mode.

No initialization is performed on this register in the PIC32 start-up code.

Trace Control Register (TraceControl – CP0 Register 23, Select 1)

This register provides control and status information. The TraceControl register is only implemented if the EJTAG Trace capability is present.

No initialization is performed on this register in the PIC32 start-up code.

Trace Control 2 Register (TraceControl2 – CP0 Register 23, Select 2)

This register provides additional control and status information. The TraceControl2 register is only implemented if the EJTAG Trace capability is present.

No initialization is performed on this register in the PIC32 start-up code.

User Trace Data Register (UserTraceData – CP0 Register 23, Select 3)

When this register is written to, a trace record is written indicating a type 1 or type 2 user format. This type is based on the UT bit in the TraceControl register. This register cannot be written in consecutive cycles. The trace output data is UNPREDICTABLE if this register is written in consecutive cycles. The UserTraceData register is only implemented if the EJTAG Trace capability is present.

No initialization is performed on this register in the PIC32 start-up code.

TraceBPC Register (TraceBPC – CP0 Register 23, Select 4)

This register is used to control start and stop of tracing using an EJTAG hardware breakpoint. The hardware breakpoint would then be set as a triggered source and optionally also as a Debug exception breakpoint. The TraceBPC register is only impl-emented if both the hardware breakpoints and the EJTAG Trace cap are present.

No initialization is performed on this register in the PIC32 start-up code.

Debug2 Register (Debug2 – CP0 Register 23, Select 5)

This register holds additional information about complex breakpoint exceptions. The Debug2 register is only implemented if complex hardware breakpoints are present.

No initialization is performed on this register in the PIC32 start-up code.

Debug Exception Program Counter (DEPC – CP0 Register 24, Select 0)

This register is a read/write register that contains the address at which processing resumes after a debug exception or Debug mode exception has been serviced. For synchronous (precise) debug and Debug mode exceptions, the DEPC contains either:

  • The virtual address of the instruction that was the direct cause of the debug exception, or
  • The virtual address of the immediately preceding branch or jump instruction, when the debug exception causing instruction is in a branch delay slot, and the Debug Branch Delay (DBD) bit in the Debug register is set.

For asynchronous debug exceptions (debug interrupt, complex break), the DEPC contains the virtual address of the instruction where execution should resume after the debug handler code is executed.

No initialization is performed on this register in the PIC32 start-up code.

Error Exception Program Counter (ErrorEPC – CP0 Register 30, Select 0)

This register is a read/write register, similar to the EPC register, except that it is used on error exceptions. All bits of the ErrorEPC are significant and must be writable. It is also used to store the program counter on Reset, Soft Reset, and Non-Maskable Interrupt (NMI) exceptions. The ErrorEPC register contains the virtual address at which instr-uction processing can resume after servicing an error. This address can be:

  • The virtual address of the instruction that caused the exception, or
  • The virtual address of the immediately preceding branch or jump instruction when the error causing instruction is a branch delay slot.

Unlike the EPC register, there is no corresponding branch delay slot indication for the ErrorEPC register.

No initialization is performed on this register in the PIC32 start-up code.

Debug Exception Save Register (DeSave – CP0 Register 31, Select 0)

This register is a read/write register that functions as a simple memory location. This register is used by the debug exception handler to save one of the GPRs that is then used to save the rest of the context to a pre-determined memory area (such as in the EJTAG Probe). This register allows the safe debugging of exception handlers and other types of code where the existence of a valid stack for context saving cannot be assumed.

No initialization is performed on this register in the PIC32 start-up code.