| 0x28 | All Xplained Pro MCU boards (I2C interface to the
embedded debugger) | Cannot be changed permanently so each reboot of the EDBG resets
this to the default address. Configuration can be done via Atmel Data
Visualizer. |
| 0x29 | BNO055 Xplained Pro | Last bit is configurable by
pull-up/down. |
| 0x4A | maXTouch Xplained Pro (mXT112S touchscreen controller) | Not configurable |
| 0x4B | ATMEGA256RFR2 Xplained Pro
(temp. sensor) | Last three bits can be
configured by soldering. This will also change the last three bits of the
EEPROM address on this board because both are within the same device. |
| 0x4F | I/O1 Xplained Pro (temp.
sensor) | Last three bits can be
configured by soldering. This will also change the last three bits of the
EEPROM address on this board because both are within the same device. |
| 0x50 | SAM L22 Xplained Pro
(ATAES132A crypto device) | Default device address. Can be
changed in internal config register. |
| 0x53 | ATMEGA256RFR2 Xplained Pro (EEPROM) | Last three bits can be
configured by soldering. This will also change the last three bits of the temp
sensor address on this board because both are within the same device. |
| 0x57 | I/O1 Xplained Pro (EEPROM) | Last three bits can be
configured by soldering. This will also change the last three bits of the temp
sensor address on this board because both are within the same device. |
| 0x70 | SHTC1 Xplained Pro | Not configurable |