27.3.2.2.4 Transmitting Data Packets
Assuming the above M1 case, the TWI master can start transmitting data by
writing to the Master Data (TWIn.MDATA) register, which will also clear the Write Interrupt
Flag (WIF). During the data transfer, the master is continuously monitoring the bus for
collisions and errors. The WIF flag will be set to ‘1’ after the data
packet transfer has been completed.
If the transmission is successful and the master receives an ACK bit from the
slave, the Received Acknowledge (RXACK) flag will be set to ‘0’, meaning
that the slave is ready to receive new data packets.
- Transmit a new data packet
- Transmit a new address packet
- Complete the transaction by issuing a Stop condition in the Command (MCMD) bit field from the Master Control B (TWIn.MCTRLB) register
If the transmission is successful and the master receives a NACK bit from the
slave, the RXACK flag will be set to ‘1’, meaning that the slave is not
able to or does not need to receive more data.
- Transmit a new address packet
- Complete the transaction by issuing a Stop condition in the Command (MCMD) bit field from the Master Control B (TWIn.MCTRLB) register
The RXACK status is valid only if the WIF flag is set to ‘1’ and the
Arbitration Lost (ARBLOST) and Bus Error (BUSERR) flags are set to ‘0’.
The transmission can be unsuccessful if a collision is detected. Then, the
master will lose arbitration, the Arbitration Lost (ARBLOST) flag will be set to
‘1’, and the bus state changes to Busy. An arbitration lost during the
sending of the data packet is treated the same way as the above M4 case.
The WIF, ARBLOST, BUSERR and RXACK flags are all located in the Master Status (TWIn.MSTATUS) register.