34.3.3.2 STS - Store Data to Data Space Using Direct
Addressing
The STS instruction is used to store data that are shifted
serially into the PHY layer shift register to the system bus address space. The
STS instruction is based on direct addressing, and the address must
be given as an operand to the instruction for the data transfer to start. The address is
the first set of operands, and data are the second set. The size of the address and data
operands are given by the size fields presented in the figure below. The maximum size
for both address and data is 32 bits.
The STS supports repeated memory access when combined with
the REPEAT instruction.
STS Instruction
OperationSTS instruction is depicted in the
above figure, following this sequence: - The address is sent.
- An Acknowledge (ACK) is sent back from the UPDI if the transfer was successful.
- The number of bytes, as specified
in the
STSinstruction, is sent. - A new ACK is received after the data have been successfully transferred.