23.3.3.2.1 One Ramp Mode
In One Ramp mode, the TCD counter counts up until it reaches the CMPBCLR value.
Then, the TCD cycle is completed, and the counter restarts from 0x000
,
beginning a new TCD cycle. The TCD cycle period is:
In the figure above, CMPASET < CMPACLR < CMPBSET < CMPBCLR.
In One Ramp mode, this is required to avoid overlapping outputs during the on time. The
figure below is an example where CMPBSET < CMPASET < CMPACLR < CMPBCLR,
which has overlapping outputs during the on time. A match with CMPBCLR will always result in all outputs being cleared. If any of
the other compare values are bigger than CMPBCLR, their associated effect will never
occur. If the CMPACLR is smaller than the CMPASET value, the clear value will not have
any effect.