1.4.1 SRAM Read-Back
Following a device power-up sequence, there is a possibility that some SRAM locations
will not return the expected written value but will read back ‘00’
instead.
Work around
None. The device can only recover by power cycling.
This erroneous condition can be detected by running the following code that writes
nonzero values to SRAM and then verifies that the returned read values are not
‘
00’. If a returned value is ‘00’, the
application code has to be put into a safe state until a POR event occurs. This code
has to be executed immediately after power-up. If the test passes, the device
operation will be
normal.// SRAM test FSR0 = 0xcff; // Write data into RAM address for devices up to 2K RAM INDF0 = 0x55; PROD = INDF0; // Read back data if (PROD == 0){ SAFE_STATE(); // RAM incorrectly read, suspend operation and go to Safe state } //For devices with more than 2K of SRAM, add the following code FSR0 = 0x14ff; // Write data into RAM INDF0 = 0x55; PROD = INDF0; // Read back data if (PROD == 0){ SAFE_STATE(); // RAM incorrectly read, suspend operation and go to Safe state } //For devices with more than 4K of SRAM, add the following code FSR0 = 0x24ff; // Write data into RAM INDF0 = 0x55; PROD = INDF0; // Read back data if (PROD == 0){ SAFE_STATE(); // RAM incorrectly read, suspend operation and go to Safe state }
Affected Silicon Revisions
| B0 | B2 | B3 | C0 |
| X |