1.3.11 I2C Module May Hang the Bus during Multi-Host Arbitration
The I2C module may hang the bus in a Multi-Host environment when another Host
device initiates a transaction on the bus by issuing the Start condition before the
I2C module pulls down the SDA line, and the most significant bit of the
address header starts with a '0' in FME=0 or
FME=1 mode.
Work around
When using FME=0 or FME=1 modes, the user can
choose to assign addresses such that the most significant bit of the address header
starts with a '1'. Alternatively, the user can select the
FME=2 mode of operation.
Affected Silicon Revisions
| B0 | B2 | B3 | C0 |
| X | X | X | X |