5.1 Preprocessor Directives
The PIC Assembler accepts several specialized preprocessor directives, in addition to the standard directives. All of these are tabulated below.
| Directive | Meaning | Example | 
|---|---|---|
# | Preprocessor null directive, do nothing. | # | 
#define | Define preprocessor macro. | 
                     
                   | 
#elif | Short for #else #if. | see #ifdef | 
#else | Conditionally include source lines. | see #if | 
#endif | Terminate conditional source inclusion. | see #if | 
#error | Generate an error message. | #error Size too big | 
#if | Include source lines if constant expression true. | 
                     
                   | 
#ifdef | Include source lines if preprocessor symbol defined. | 
                     
                   | 
#ifndef | Include source lines if preprocessor symbol not defined. | 
                     
                   | 
#include | Include text file into source. | 
                     
                   | 
#line | Specify line number and filename for listing | #line 3 final | 
#nn filename | (where nn is a
                     number, and filename is the name of the source file)
                     the following content originated from the specified file and line
                     number. | #20 init.c | 
#undef | Undefines preprocessor symbol. | #undef FLAG | 
#warning | Generate a warning message. | #warning Length not
                     set | 
Macro expansion using arguments can use the # character
         to convert an argument to a string and the ## sequence to concatenate
         arguments. If two expressions are being concatenated, consider using two macros in case
         either expression requires substitution itself; for example
#define __paste1(a,b)   a##b
#define __paste(a,b)    __paste1(a,b)lets you use the paste macro to concatenate two
         expressions that themselves can require further expansion. Remember, that once a macro
         identifier has been expanded, it will not be expanded again if it appears after
         concatenation.