5.6.3 Symbol Table
At the bottom of each assembly list file is a symbol table. This differs from the symbol table presented in the map file (see Symbol Table) in two ways:
- Only symbols associated with the assembly module, from which the list file is produced (as opposed to the entire program) are listed.
- Local as well as global symbols associated with that module are listed.
Each symbol is listed along with the address it has been assigned.