7.2.3.16 Find and Replace Hexmate Option
If the replace form of the -find option
(see Find Hexmate Option) is used, any
matching sequences will be replaced, or partially replaced, with new codes.
To have the
-find option perform replacement, append
,replace=spec to the option in the following
manner.-find=spec,replace=Code[mMask]where:Codeis a hexadecimal code sequence to replace the sequences that match the-findcriteria.Maskis an optional bit mask to specify which bits withinCodewill replace the code sequence that has been matched. This can be useful if, for example, it is only necessary to modify 4 bits within a 16-bit instruction. The remaining 12 bits can masked and left unchanged.
For
example:
-find=ff@7fe0-7fff,replace=55Attention: This function should be used with extreme caution
and is not normally recommended for the replacement of data or executable code.