6.3.2 Contents
The sections in the map file, in order of appearance, are as follows.
- The assembler name and version number.
- A copy of the command line used to invoke the linker.
- The version number of the object code in the first file linked.
- The machine type.
- A psect summary sorted by the psect’s parent object file.
- A psect summary sorted by the psect’s CLASS.
- A segment summary.
- Unused address ranges summary.
- The symbol table.
- Information summary for each function.
- Information summary for each module.
Portions of an example map file, along with explanatory text, are shown in the following sections.