6.1 Operation
hlink [options] filesThe options are zero or more
case-insensitive linker options, each of which modifies the behavior of the linker in some
way. The files is one or more object files and zero or
more library files (.a extension).
The options recognized by the linker are listed in the table below and are discussed in the paragraphs that follow.
| Option | Effect |
|---|---|
-Aclass=low-high
,... | Specify address ranges for a class. |
-Cpsect=class | Specify a class name for a global psect. |
-Ctype | Specify call graph type. |
-Dclass=delta | Specify a class delta value. |
-Dsymfile | Produce old-style symbol file. |
-Eerrfile | Write error messages to errfile. |
-F | Produce .o file with only
symbol records. |
-G
spec | Specify calculation for segment selectors. |
-H
symfile | Generate symbol file. |
-H+
symfile | Generate enhanced symbol file. |
-I | Ignore undefined symbols. |
-J
num | Set maximum number of errors before aborting. |
-K | Prevent overlaying function parameter and auto areas. |
-L | Preserve relocation items in .o file. |
-LM | Preserve segment relocation items in
.o file. |
-Mmapfile | Generate a link map in the named file. |
-N | Sort symbol table in map file by address order. |
-Nc | Sort symbol table in map file by class address order. |
-Ns | Sort symbol table in map file by space address order. |
-Ooutfile | Specify name of output file. |
-Pspec | Specify psect addresses and ordering. |
-Qprocessor | Specify the device type (for cosmetic reasons only). |
-S | Inhibit listing of symbols in symbol file. |
-Sclass=limit[,bound] | Specify address limit, and start boundary for a class of psects. |
-Usymbol | Pre-enter symbol in table as undefined. |
-Vavmap | Use file avmap to generate an Avocet format symbol file. |
-Wwarnlev | Set warning level (-9 to 9). |
-Wwidth | Set map file width (>=10). |
-X | Remove any local symbols from the symbol file. |
-Z | Remove trivial local symbols from the symbol file. |
--DISL=list | Specify disabled messages. |
--EDF=path | Specify message file location. |
--EMAX=number | Specify maximum number of errors. |
--fixupoverflow=action | Specify response when encountering fixup overflows. |
--NORLF | Do not relocate list file. |
--VER | Print version number and stop. |
--werror=num | Promote warnings to errors |
\ at the
end of the preceding line. In this fashion, hlink commands of almost
unlimited length can be issued. For example, a link command file called
x.lnk and containing the following
text:-Z -Ox.o -Mx.map \
-Ptext=0,data=0/,bss,nvram=bss/. \
x.o y.o z.ocan be passed to the linker by one of the
following:hlink @x.lnk
hlink < x.lnkSeveral linker options require memory addresses or sizes to be specified.
The syntax for all of these is similar. By default, the number is interpreted as a decimal
value. To force interpretation as a HEX number, a trailing H, or
h, should be added. For example, 765FH will be treated
as a HEX number.
To build projects you will typically use either the MPLAB XC8 C compiler
(xc8-cc) driver or the MPLAB XC8 PIC Assembler
(pic-as) driver. These will call the linker for you, passing it a
set of default linker options. If you need to modify or supply additional linker options
when using a driver, use either the -Wl (see Wl: Pass Option To The Linker,
Option) or
-Xlinker (see Xlinker Option) driver options, which will pass on the suboption to the linker
application when it is executed.