3.4.32 W: Enable or Disable Message Option

The -Wmsg option enables warning and advisory messages. The msg argument can be the name of a message issued by Clang (e.g. implicit-int) or the number of a message issued by any other compiler application (e.g. 2102). The special message argument all indicates that all messages should be enabled. This option has precedence over the -w option, which disables all warning messages, so it can be used to re-enable selected messages when -w has been used.

The -Wno-msg form of the option disables the indicated message, using the same arguments as the enabling form of this option. Where the msg argument corresponds to a warning or advisory message, this message will never be issued by the compiler or assembler. If the argument corresponds to an error or is not recognized, the compiler will indicate via an error that this operation is not permitted.

The name of the message is printed in Clang warnings (as shown in the following example of a return-type warning).
main.c:12:1: warning: control reaches end of non-void function [-Wreturn-type]

In the case where -Wno-msg has been issued and msg is a number that corresponds to a warning that has been promoted to an error through the -Werror option, then that message will not be issued by the compiler, nor will any error corresponding to that message.

Where the #pragma warning has been used in code, it will override at the appropriate time of compilation the actions of the -Wno-msg and -Werror options.

If both the -mwarn and -W[no-]msg options have been specified, they are processed in the order in which they appear on the command line.