1.17.4 Erase Flash Command
This command erases the number of flash PAGES in the length field. The actual size of the page depends upon the device being programmed. The address must be the beginning address of the first page to be programmed. In addition, attempting to erase memory outsize the application space will result in a Invalid Address (0xFE) status. The correct unlock sequence must be sent to the part for each command as it is not stored on the device
|
Field Size |
Description |
Data Type |
Comments | |
|---|---|---|---|---|
|
1 |
Cmd |
uint8_t |
Command (0x03) - Erase Program Memory | |
|
2 |
Length |
uint16_t |
Number of pages to erase. Low Byte First | |
|
4 |
Unlock Seqeunce |
uint32_t |
Unlock sequence for flash. Key for currently supported parts is 0x00AA0055 | |
|
4 |
Address |
uint32_t |
Address of the first memory location to erase. Must be page aligned. Low byte first. |
Erase Command Response Format
|
Field Size |
Description |
Data Type |
Comments | |
|---|---|---|---|---|
|
1 |
Cmd |
uint8_t |
Command (0x03) - Erase Program Memory | |
|
2 |
Length |
uint16_t |
Number of pages to erase. Low Byte First | |
|
4 |
Unlock Seqeunce |
uint32_t |
Unlock sequence for flash. Key for currently supported parts is 0x00AA0055 | |
|
4 |
Address |
uint32_t |
Address of the first memory location to erase. Must be page aligned. Low byte first. | |
|
1 |
Status |
uint8_t |
Status of Command
|
Example Sequence
Erase two pages of flash starting at address 0x000A000. All values in Hex
Example command to the device
|
Field Size |
Description |
Data Type |
Value | |
|---|---|---|---|---|
|
1 |
Cmd |
uint8_t |
0x03 | |
|
2 |
Length |
uint16_t |
0x0002 | |
|
4 |
Unlock Seqeunce |
uint32_t |
0x00AA0055 | |
|
4 |
Address |
uint32_t |
0x00A000 |
Example as viewed on bus: 0x03, 0x02, 0x00, 0x55, 0x00, 0xAA, 0x00, 0x00, 0xA0, 0x00, 0x00
<erase_command_example_response Erase Example Response Sequence
Example reponse from the device
|
Field Size |
Description |
Data Type |
Value | |
|---|---|---|---|---|
|
1 |
Cmd |
uint8_t |
0x01 | |
|
2 |
Length |
uint16_t |
0x0002 | |
|
4 |
Unlock Seqeunce |
uint32_t |
0x00AA0055 | |
|
4 |
Address |
uint32_t |
0x00A000 | |
|
1 |
Status |
uint32_t |
0x01 |
Example as viewed on bus: 0x03, 0x02, 0x00, 0x55, 0x00, 0xAA, 0x00, 0x00, 0xA0, 0x00, 0x00, 0x01