1.17.3 Write Flash Command
This command will program the flash with the data in the payload section. The address and size of the payload will be inspected by the bootloader to prevent accidental over-write of protected spaces. Attempts to write into the memory where the bootloader or configuration bits resides will be prevented and an error will be returned. The flash architecture also places limitations on the address alignment and size of the requests. The start address must always be on an Min Write Size aligned address and its length must also be modulus the Min Write Size in bytes. If either address or length is not aligned the device will not write the data and a status of 0xFE (Invalid Address) will be returned. The user is responsible for erasing flash before writing. Failure to do so will have unexpected results. The correct unlock sequence must be sent to the part for each command as it is not stored on the device
|
Field Size |
Description |
Data Type |
Comments | |
|---|---|---|---|---|
|
1 |
Cmd |
uint8_t |
Command (0x02) - Write Program Memory | |
|
2 |
Length |
uint16_t |
Number of bytes to program. Must be evenly divisible by the Minimum Write Size parameter in the Get Version response. Command will return error if it's not evenly divisible | |
|
4 |
Unlock Seqeunce |
uint32_t |
Unlock sequence for flash. Key for currently supported parts is 0x00AA0055 | |
|
4 |
Address |
uint32_t |
Address of the first memory location to program. Must be aligned to the Minimum Write Size parameter in the Get Version response. Command will return error if it's not aligned | |
|
Variable |
Data To Write |
uint8_t |
Seqeunce of bytes. Data to write |
Write Command Response Format
|
Field Size |
Description |
Data Type |
Comments | |
|---|---|---|---|---|
|
1 |
Cmd |
uint8_t |
Command (0x02) - Write Program Memory | |
|
2 |
Length |
uint16_t |
Number of bytes to write. | |
|
4 |
Unlock Seqeunce |
uint32_t |
Unlock sequence for flash. Key for currently supported parts is 0x00AA0055 | |
|
4 |
Address |
uint32_t |
Address of the first memory location to write. Must be aligned to and modulus of the Minimum Write Size. | |
|
1 |
Status |
uint8_t |
Status of Command
|
Write_Example Command
Write 8 bytes of data (0x01,0x02,0x03,0x04,0x05,0x06,0x07,0x08) starting at address 0x00001878. All values in Hex
Example command to the device
|
Field Size |
Description |
Data Type |
Value | |
|---|---|---|---|---|
|
1 |
Cmd |
uint8_t |
0x02 | |
|
2 |
Length |
uint16_t |
0x0008 | |
|
4 |
Unlock Seqeunce |
uint32_t |
0x00AA0055 | |
|
4 |
Address |
uint32_t |
0x00001878 | |
|
8(for this example) |
Data to write |
uint8_t |
0x01,0x02,0x03,0x04,0x05,0x06,0x07,0x08 |
Example as viewed on bus: 0x02, 0x08, 0x00, 0x55, 0x00, 0xAA, 0x00, 0x78, 0x18, 0x00, 0x00, 0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x07, 0x08
Example reponse from the device
|
Field Size |
Description |
Data Type |
Value | |
|---|---|---|---|---|
|
1 |
Cmd |
uint8_t |
0x02 | |
|
2 |
Length |
uint16_t |
0x0008 | |
|
4 |
Unlock Seqeunce |
uint32_t |
0x00AA0055 | |
|
4 |
Address |
uint32_t |
0x00001878 | |
|
1 |
Status |
uint32_t |
0x01 |
Example as viewed on bus: 0x02, 0x08, 0x00, 0x55, 0x00, 0xAA, 0x00, 0x78, 0x18, 0x00, 0x00, 0x01