7.11 Issue message transmitted with wrong arbitration and control fields
- M_CAN is in state "Receiver" (PSR.ACT = "10") and there is no pending transmission.
- A new transmission is requested before the third Intermission bit is reached.
- The CAN bus is sampled dominant at the third Intermission bit which is treated as SoF (see ISO11898-1:2015 Section 10.4.2.2).
Then, it can happen that:
- The Shift register is not loaded with the ID, format and DLC of the requested message.
- The MCAN starts arbitration with wrong ID, format, and DLC on the next bit.
- If the ID wins arbitration, a CAN message with valid CRC is transmitted.
- If this message is acknowledged, the ID stored in the Tx Event FIFO is the ID of the requested Tx message, and not the ID of the message transmitted on the CAN bus, and no error is detected by the transmitting MCAN.
Work Around
Request a new transmission only if another transmission is already pending or when the MCAN is not in "Receiver" state (when PSR.ACT ≠ "10").
To avoid activating the transmission request in the critical time window between the sample points of the second and third Intermission bits, the application software can evaluate the Rx Interrupt flags IR.DRX, IR.RF0N and IR.RF1N, which are set at the last EoF bit when a received and accepted message becomes valid.
The last EoF bit is followed by three Intermission bits. Therefore, the critical time window has safely terminated three bit times after the Rx interrupt. Now a transmission can be requested by writing to TXBAR.
After the interrupt, the application has to take care that the transmission request for the CAN Protocol Controller is activated before the critical window of the following reception is reached.
A checksum covering the arbitration and control fields can be added to the data field of the message to be transmitted, to detect frames transmitted with wrong arbitration and control fields.