3.3.12.1 READ_MODE

Setting READ_MODE to 1 indicates to the SMC that the NRD signal is responsible for turning off the tri-state buffers of the external memory device. The Data Float Period then begins after the rising edge of the NRD signal and lasts TDF_CYCLES MCK cycles.

When the read operation is controlled by the NCS signal (READ_MODE = 0), the TDF field shows the number of MCK cycles during which the data bus remains busy after the rising edge of NCS.

Figure 3-29 illustrates the Data Float Period in NRD-controlled mode (READ_MODE = 1), assuming a data float period of two cycles (TDF_CYCLES = 2). Figure 3-30 shows the read operation when controlled by NCS (READ_MODE = 0) and the TDF_CYCLES parameter equals 3.

Figure 3-29. TDF Period in NRD Controlled Read Access (TDF = 2)
Figure 3-30. TDF Period in NCS Controlled Read Operation (TDF = 3)