Normal mode configures the SAM-BA Monitor to send/receive data
in binary format.
Terminal mode configures the SAM-BA Monitor to send/receive data
in ASCII format.
Write commands: Writes a byte (O), a halfword (H) or a
word (W) to the target.
Address: address in hexadecimal
Value: byte, halfword or word to write in hexadecimal
Output: ‘>’
Read commands: Reads a byte (o), a halfword (h) or a
word (w) from the target.
Address: address in hexadecimal
Output: the byte, halfword or word read in hexadecimal followed
by ‘>’
Send a file (S): The host will send a buffer of data to be
stored at a specified address in the device
Address: address in hexadecimal
NbOfBytes: number of bytes (in hexadecimal format) to be received from the
host
Output: ‘>’
Note: A timeout on
this command is reached when the prompt ‘>’ appears before the end of the
command execution.
Receive a file (R): The host requests to read a buffer of data
from a specified address in the device.
Address: address in hexadecimal
NbOfBytes: number of bytes (in hexadecimal format) to be sent to
the host
Output: ‘>’
Go (G): Jumps to a specified address and executes the code.
Address: address to jump to in hexadecimal
Output: ‘>’ once returned from the program execution. If the
executed program does not manage the link register and does not return, the prompt
is not displayed.
Get ROM code version (V): Returns the ROM code version.
Output: version, date and time of ROM code followed by
‘>’
DS60001813E
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.