5.2.6.12.1 Input-Output Transfer Functions

The ADC can be configured to operate in the following input voltage modes:

  • Single-Ended—ADC_CCR.DIFFx = 0 and ADC_PDR.PDIFFx = 0. This is the default mode after a reset.
  • Differential—ADC_CCR.DIFFx = 1 and ADC_PDR.PDIFFx = 0 (see the figure below). In Differential mode, the ADC requires differential input signals having a VDD/2 common mode voltage (refer to the section “Electrical Characteristics”).
  • • Pseudo-Differential—ADC_PDR.PDIFFx = 1. In Pseudo-Differential mode, one of the analog pins is used as the negative input of the ADC (see table Input Pins and Channel Numbers in Pseudo-Differential Mode). The ADC samples the other analog inputs with respect to this one. The common mode input range is 0 to VDD (refer to the section “Electrical Characteristics”).

The following equations provide the unsigned ADC input-output transfer function in each mode(1). With signed conversions (see field ADC_EMR.SIGNMODE), subtract 2047 from the ADC_LCDR.DATA value given below. Note that the Single-Ended mode introduces a x2 gain compared to the Pseudo-Differential mode.

In the formula, REFP = VREFP, REFN = VREFN.

Single-Ended mode:

ADC_LCDR.LDATA=ADx−REFNREFP−REFN×212

Differential mode:

ADC_LCDR.LDATA=1+ADx−ADx+1REFP−REFN×211

Pseudo-Differential mode:

ADC_LCDR.LDATA=1+ADx−AD7REFP−REFN×211
Note: Equations assume ADC_EMR.OSR = 1

If ADC_MR.ANACH is set, the ADC can manage both differential channels and single-ended channels. If ADC_MR.ANACH is cleared, the parameters defined in ADC_CCR are applied to all channels.

The following tables provide the internal positive and negative ADC inputs assignment with respect to the programmed mode (ADC_CCR.DIFFx and ADC_PDR.PDIFFx).

For example, if Differential mode is required on channel 0, input pins AD0 and AD1 are used. In this case, only channel 0 must be enabled by writing a 1 to ADC_CHER.CH0.

Table 5-2. Input Pins and Channel Numbers in Single-Ended and Differential Modes
Internal ADC Inputs (VIN+, VIN-)Channel Number
Single-Ended ModeDifferential ModeSingle-Ended ModeDifferential Mode
AD0, ADVREFNAD0, AD1CH0CH0
AD1, ADVREFN–CH1
AD2, ADVREFNAD2, AD3CH2CH2
AD3, ADVREFN–CH3
AD4, ADVREFNAD4, AD5CH4CH4
AD5, ADVREFN–CH5
AD6, ADVREFNAD6, AD7CH6CH6
AD7, ADVREFN–CH7

In Pseudo-Differential mode, inputs are managed by a 8/2:1-channel analog multiplexer. See the table below.

Table 5-3.  Input Pins and Channel Numbers in Pseudo-Differential Mode
Internal ADC Inputs (VIN+, VIN-)Channel Number
AD0, AD7CH0
AD1, AD7CH1
AD2, AD7CH2
AD3, AD7CH3
AD4, AD7CH4
AD5, AD7CH5
AD6, AD7CH6
GNDANA, AD7CH7
Figure 5-7. Analog Full Scale Ranges in Single-Ended/Pseudo-Differential/Differential Applications