3.1.2.2 Operating System Support
On Windows® machines, the CDC will enumerate as Curiosity Virtual COM Port and appear in the Ports section of the Windows Device Manager. The COM port number can also be found there.
Info: On older Windows
systems, the CDC requires a USB driver. Both MPLAB X
IDE and Microchip Studio installationsinclude this driver.
On Linux® machines, the CDC will enumerate and appear as /dev/ttyACM#.
Info: tty* devices belong to the “dialout” group in Linux, so it may be necessary to become a member of that group to have permission to access the CDC.
On Mac® machines, the CDC will enumerate and appear as /dev/tty.usbmodem#. Depending on the terminal program used, it will appear in the available list of modems as usbmodem#.
Info: For all operating systems, use a terminal emulator that supports DTR signaling. See Signaling.