Introduction

This user guide provides detailed information about using the Microchip Radio Test 3 tool (MCHPRT3) with the Microchip RNBD. The MCHPRT3 enables the user to evaluate and demonstrate the RF performance of the RNBD.

Note: In this user guide, the MCHPRT3 tool with the RNBD Add-on Board is only shown as an example.

The MCHPRT3 is intended for development purposes. Any production test must use either a third-party production tool or users must develop their own production tool based on the DLL release.