11 Appendix C: Command Summary Quick Reference
The following table summarizes the ASCII commands.
| ASCII Command | Version 1.0 | Version 1.2 and later | Description |
|---|---|---|---|
| System Configuration | |||
SS | ✔ | ✔ | Set Service Configure |
SSC | ❌ | ✔ | Default Service Configure |
GK | ✔ | ✔ | Get Connection Status |
QCCS | ❌ | ✔ | Query Current Connection Status |
+ | ✔ | ✔ | Echo |
$$$ | ✔ | ✔ | Enter Command Mode |
--- | ✔ | ✔ | Exit Command Mode |
S$ | ✔ | ✔ | Set Enter Command Character |
S% | ✔ | ✔ | Set Status Delimiter |
G<char> | ✔ | ✔ | Get Configuration |
V | ✔ | ✔ | Query Firmware Version |
VER | ❌ | ✔ | |
D | ✔ | ✔ | Get Local Information |
DINF | ❌ | ✔ | Device Information |
! | ✔ | ✔ | Remote Command Mode Control |
RMT | ❌ | ✔ | Enter/Exit Remote Command Mode |
SF,<1,2> | ✔ | ✔ | Factory Reset |
FR,<1,2> | ❌ | ✔ | |
O | ✔ | ✔ | Shutdown |
OFF | ❌ | ✔ | Shut Down Device |
R,1 | ✔ | ✔ | Reboot |
RST | ❌ | ✔ | Reset the Device |
SR | ✔ | ✔ | Set Application Options |
SAO | ❌ | ✔ | |
SLOG | ✔ | ✔ | Set Debug Log |
GLOG | ✔ | ✔ | Get Debug Log Setting |
VOS | ✔ | ✔ | Get Silicon Version |
SVD | ✔ | ✔ | Set Vendor Data |
GVD | ✔ | ✔ | Get Vendor data |
SW | ✔ | ✔ | Set Pin Function |
GW
| ✔ | ✔ | Get Pin Function |
SPTA
| ✔ | ✔ | Set PTA |
GPTA
| ✔ | ✔ | Get PTA Setting |
SH | ✔ | ✔ | Set HCI Determination |
SCHI | ❌ | ✔ | Set HCI |
| GAP – General | |||
S- | ✔ | ✔ | Set Device Name With Address |
SNA | ❌ | ✔ | Set Name with Address |
SN | ✔ | ✔ | Set Device Name |
GNR | ✔ | ✔ | Get Remote Device Name |
SGA | ✔ | ✔ | Set RF Power in Advertisement |
SGC | ✔ | ✔ | Set RG Power in Connected State |
M | ✔ | ✔ | Get Signal Strength |
QRSS | ❌ | ✔ | Query Received Signal Strength |
SO | ✔ | ✔ | Low Power Control |
SPD | ❌ | ✔ | Set Power Down |
MTP | ✔ | ✔ | Read Local TX Power |
MRTP | ✔ | ✔ | Read Remote TX Power |
| GAP – Advertising | |||
A | ✔ | ✔ | Start Advertisement |
IA/IS/NA/NS | ✔ | ✔ | Set Advertisement Data |
IAE/NAE/ISE/NSE | ✔ | ✔ | Set Extended Advertisement Data |
IPE | ✔ | ✔ | Set Extended Advertisement Parameter |
IRA | ✔ | ✔ | Get Local Advertisement Address |
QAA | ❌ | ✔ | Query Advertising Address |
STA | ✔ | ✔ | Set Fast Advertisement Parameter |
DA | ❌ | ✔ | Disable Advertising |
Y | ✔ | ✔ | Stop Advertising |
SDO | ✔ | ✔ | Set Deep Sleep Advertising |
SDSA | ✔ | ✔ | Set Deep Sleep Advertisement |
GDO | ✔ | ✔ | Get Deep Sleep Advertising Parameters |
GDSA | ❌ | ✔ | |
IB/NB | ✔ | ✔ | Set Beacon Data Immediately |
STB | ✔ | ✔ | Set Beacon Advertising Parameter |
SPB | ❌ | ✔ | Set Beacon Parameter |
GPB | ✔ | ✔ |
Get Beacon Advertisement Parameter |
GTB | ❌ | ✔ | Get Beacon Parameter |
SC | ✔ | ✔ |
Set Advertisement Enable Configuration |
SAC | ❌ | ✔ | Set Advertising Configuration |
GC | ✔ | ✔ |
Get Advertisement Enable Configuration |
GAC | ❌ | ✔ | Get Advertising Configuration |
| GAP – Scan | |||
F | ✔ | ✔ | Start Bluetooth® Low Energy Scanning |
FE | ✔ | ✔ | Start Extended Bluetooth Low Energy Scanning |
X | ✔ | ✔ | Stop Bluetooth Low Energy Scanning |
DF | ❌ | ✔ | Disable Finding |
| GAP – Connection | |||
ST | ✔ | ✔ | Set Central Initial Connection Parameter |
SICP | ❌ | ✔ | Set Initial Connection Parameter |
T | ✔ | ✔ | Request Connection Parameter Update |
UCP | ❌ | ✔ | Update Connection Parameter |
C | ✔ | ✔ | Connect Last Bonded Device |
C,<0,1>,<address> | ✔ | ✔ | Connect Device by Address |
C<1-8> | ✔ | ✔ | Connect Specific Bonded Device |
CE | ✔ | ✔ | Connect Device with Extended Parameter |
CSPHY | ✔ | ✔ | Set PHY Preference |
CRPHY | ✔ | ✔ | Get PHY Preference |
K,1 | ✔ | ✔ | Disconnect Link |
DISC | ❌ | ✔ | Disconnect |
Z | ✔ | ✔ | Cancel Create Connection |
CCC | ❌ | ✔ | Cancel Creating Connection |
| GAP – Security | |||
SA | ✔ | ✔ | Set Pairing Mode |
SP | ✔ | ✔ | Set Fixed Pin Code |
B | ✔ | ✔ | Start Bonding Process |
JA | ✔ | ✔ | Add One Device Into Accept List |
ALA | ❌ | ✔ | Accepted List by Address |
JB | ✔ | ✔ | Add Bonded List Into Accept List |
ALB | ❌ | ✔ | Accepted List by Bonded Device |
JC | ✔ | ✔ | Clear Accept List |
ALC | ❌ | ✔ | Accepted List Clear |
JD | ✔ | ✔ | Display Accept List |
ALD | ❌ | ✔ | Accepted List Display |
U | ✔ | ✔ | Unbond Device |
UB | ❌ | ✔ | Unbond |
LB | ✔ | ✔ | List All Bonded Devices |
&SEP | ✔ | ✔ | Enable/Disable Local Privacy |
SLP | ❌ | ✔ | Set Local Privacy |
&SGP | ✔ | ✔ | Get Local Privacy setting |
GLP | ❌ | ✔ | Get Local Privacy |
SPW | ✔ | ✔ | Set Remote Command Mode Password |
GPW | ✔ | ✔ | Get Remote Command Mode Password |
| GATT – Generic Access Service Setting | |||
SDA | ✔ | ✔ | Set Appearance |
SAPR | ❌ | ✔ | |
| GATT – Device Information Service Setting | |||
SDF | ✔ | ✔ | Set Firmware Version |
SDH | ✔ | ✔ | Set Hardware Version |
SDM | ✔ | ✔ | Set Model Name |
SDN | ✔ | ✔ | Set Manufacturer Name |
SDR | ✔ | ✔ | Set Software Revision |
SDS | ✔ | ✔ | Set Serial Number |
| GATT – GATT Operation on Server Role | |||
PC | ✔ | ✔ | Define Service Characteristic |
SPC | ❌ | ✔ | Set Proprietary Characteristic |
PS | ✔ | ✔ | Define Service UUID |
SPS | ❌ | ✔ | Set Proprietary Service |
PZ | ✔ | ✔ | Clear Customized Services |
SPSN | ❌ | ✔ | Set Proprietary Service Null |
LS | ✔ | ✔ | List Customized Service |
LPS | ❌ | ✔ | List Private Services |
SI | ✔ | ✔ | Service Changed Indication |
ISC | ❌ | ✔ | Indicate Service Change |
SHR | ✔ | ✔ | Read Local Characteristic Value |
QSH | ❌ | ✔ | Query Server Handle |
SHW | ✔ | ✔ | Write Local Characteristic Value |
SHWM | ✔ | ✔ | Write Local Characteristic Value for Multiple Links |
| GATT – GATT Operation on Client Role | |||
CHR | ✔ | ✔ | Read Remote Characteristic Value |
QCH | ❌ | ✔ | Query as Client by Handle |
CHW | ✔ | ✔ | Write Remote Characteristic Value |
CHWM | ✔ | ✔ | Write Remote Characteristic Value for Multiple Links |
CI | ✔ | ✔ | Discovery Remote Services |
QCS | ❌ | ✔ | Query as Client by Service |
LC | ✔ | ✔ | List Remote Services |
LCM | ✔ | ✔ | List Remote Services for Specific Link |
| Data Transmission For Multi-link | |||
IE | ✔ | ✔ | Send Transparent Data |
| Peripheral Commands | |||
SB | ✔ | ✔ | Set UART Baud Rate |
SBR | ❌ | ✔ | Set Baud Rate |
SBI | ✔ | ✔ | Set UART Baud Rate Immediately |
SBRI | ❌ | ✔ | |
|I | ✔ | ✔ | Set Digital Input and Read Port |
QIO | ❌ | ✔ | Query Digital I/O Port |
|O | ✔ | ✔ | Set Digital Output Port |
WIO | ❌ | ✔ | Write Digital I/O Port |
EIM | ✔ | ✔ | Set Event Indication Mask |
SEIM | ❌ | ✔ | |
GEI | ✔ | ✔ | Get Event Indication Value |
QEI | ❌ | ✔ | Query Event Indication |
SIL | ✔ | ✔ | Set Link Quality Indication |
SLQI | ❌ | ✔ | |
GIL | ✔ | ✔ | Get Link Quality Indication Setting |
GLQI | ❌ | ✔ | Get Link Quality Indication |
@,4 | ✔ | ✔ | Read ADC Input Voltage |
QBV | ❌ | ✔ | Query Battery Voltage |
S@ | ✔ | ✔ | Set ADC Reference Factors |
SBVF | ❌ | ✔ | Set Battery Voltage Factors |
SPMU | ✔ | ✔ | Set PMU Mode |
GPMU | ✔ | ✔ | Get PMU Mode Status |
STI | ✔ | ✔ | Set UART TX Indication |
GTI | ✔ | ✔ | Get UART TX Ind Setting |
DTM | ✔ | ✔ | Enable Device Test Mode |
DFU | ✔ | ✔ | Enter DFU Mode |
DFUU | ✔ | ✔ | DFU Update Request |
DFUS | ✔ | ✔ | DFU Update Start |
DFUD | ✔ | ✔ | DFU Image Distribution |
DFUC | ✔ | ✔ | DFU Update Complete |
DFUE | ✔ | ✔ | Terminate DFU Operation |
OTAV | ✔ | ✔ | Host MCU notify RNBD350 the Validation Status |
OTAA | ✔ | ✔ | Allow OTA DFU or MCU Request RNBD350 Continue Transmit Payload Fragment |