5 Code Examples
The example application is based on the Atmel AVR Software Framework that is included in Atmel Studio 6. The AVR Software Framework can also be found as a separate package online at:
http://www.atmel.com/tools/avrsoftwareframework.aspx.
For more information about the code example, see the application note Atmel AT02657 XMEGA-E5 Xplained Software Users Guide.
The Atmel AT32UC3B1256 board controller is also pre-programmed with a bootloader and a USART-to-USB gateway application, which can be used to communicate with the target controller ATxmega32E5.