1 Harmony 3 Driver and System Service Application Examples for SAM D20 Family
The following applications are provided to demonstrate the typical or interesting usage
models of one or more drivers, system services and RTOS.
| Name | Description |
|---|---|
| Console Debug System Service using UART | This example application demonstrates the UART based console and debug system service |
| FAT Filesystem using NVM Media | This application shows an example of implementing a FAT disk in the device internal Flash memory |
| FreeRTOS Basic | This example application demonstrates context switching between four tasks of different priorities. Two tasks run periodically while the other two tasks are event driven |
| I2C Driver Asynchronous - Multi Client | This example application demonstrates the multi-client feature of the asynchronous mode of the I2C driver by communicating with an external EEPROM and a temperature sensor |
| I2C EEPROM AT24 Driver - EEPROM Read Write | This example application demonstrates how to use the AT24 driver to perform read and write operations on AT24 series of EEPROM |
| SPI Driver Asynchronous - Self Loopback Multi Client | This example demonstrates the multi client feature of the SPI driver by performing self-loop back with two clients connected on the same SPI bus |
| SPI EEPROM AT25 Driver - EEPROM Read Write | This example application demonstrates how to use the AT25 driver to perform read and write operations on AT25 series of EEPROM |
| Time System Service Multi-client | This example application demonstrates the multi-client system timer functionality |
| USART Driver Asynchronous - USART Multi Instance | This example application demonstrates the multi instance feature of the asynchronous mode of the USART driver |