1.4 ADC Sample
This example application shows how to sample an analog input using the ADC and displays the converted samples on a serial terminal.
Description
In this application, DAC output is fed to an analog input for the ADC conversion. An analog input is converted by a software trigger and the converted value is displayed on the console. DAC output is changed by 0.1V upon switch press.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/adc/adc_sample/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description | 
|---|---|
| sam_e54_xpro.X | MPLABX project for SAM E54 Xplained Pro Evaluation Kit | 
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description | 
|---|---|
| sam_e54_xpro.X | SAM E54 Xplained Pro Evaluation Kit | 
Setting Up SAM E54 Xplained Pro Evaluation Kit
- Analog input (AIN1 - PA03) of the ADC is fed from the DAC0 output(VOUT[0] -
                            PA02)
- PA03 is routed to pin 4 of the EXT2 header
 - PA02 is routed to pin 1 of the ADC/DAC Header
 
 - Use a jumper wire (male to female) to connect pin 1 of ADC/DAC Header to pin 4 of EXT2
 - Connect the Debug USB port on the board to the computer using a micro USB cable
 
Running the Application
- Open the Terminal application (Ex.:Tera term) on the computer
 - Connect to the EDBG Virtual COM port and configure the serial settings as
                        follows:
- Baud : 115200
 - Data : 8 Bits
 - Parity : None
 - Stop : 1 Bit
 - Flow Control : None
 
 - Build and Program the application using its IDE
 - Press switch to change the DAC value
 - ADC input voltage changes by 0.1 V when the switch is pressed, from 1.2V to 2.4V
 - Refer to the table below for the switch details:
Board Switch Name SAM E54 Xplained Pro Evaluation Kit SW0  - Console displays the ADC count and the ADC input voltage in the console as shown
                        below: